Compressed air is one the most important industrial energy sources. In Germany alone, some 62,000 pneumatic installations are in operation. Not infrequently, however, these installations do not include any monitoring facilities – a serious error, since 79% of the costs of compressed air are accounted for by the electricity used for generation and preparation. Even if compressors, distribution systems and pneumatic actuators are correctly dimensioned, leakage often causes losses of up to 600 l/min. What does it matter, it’s only air, users might think. But even a reduction of compressed-air losses of 100 l/min. saves up to 1000 euros a year.

However, users often fail to exploit this potential for savings due to lack of know-how. Furthermore, in many cases the technical equipment necessary to localise losses is not available. Frequently, lack of time and clarity regarding operational responsibilities prevent the implementation of energy-saving measures. This is precisely where that Festo Energy Saving Services come into play. They can help to monitor and optimise compressed air consumption by simple means. These services always begin with a report thoroughly describing the actual situation and an analysis of the complete pneumatic installation in question in order to identify all the weaknesses, from the compressor through to the applications.


Reducing energy costs
With optimum leak management, costs drivers have no chance of escaping detection. Each leakage point which is eliminated has an immediate effect in reducing compressed-air costs. According to a study by the Fraunhofer Institute ISI (“Compressed Air Systems in the European Union”, 2000), the elimination of leaks alone enables around 42% of total potential savings to be achieved. As part of an efficient leak-management system, a specialist will use an ultrasound detector to check the compressed air system for leaks and will record each leak together with all the associated technical data, such as details of the spare parts required. This documentation will then serve as a master plan for possible savings. This will show all the required maintenance measures and lists the long-term savings against the short-term repair costs.

优化压缩空气消耗量

越来越多的公司将精确的压缩空气消耗量数据作为选择新设备的主要标准。通过对压缩空气消耗量进行详细分析,与传统方法相比,公司可以节省多达 50% 的费用。即使在调试之前,进行压缩空气消耗量分析也有助于确定设备的精确压缩空气消耗量,其中包括正常运行期间和机器处于静止状态时的数据。因此,此举可以保证压缩空气供应系统具有最佳尺寸,同时防止由于过载而导致供应系统崩溃。尤为重要的是,压缩空气消耗量分析从一开始就避免了不必要的成本,即由于系统尺寸过大以及由此造成的压缩空气分配系统价格过高而产生的成本。

延长使用寿命

最佳的压缩空气质量可以确保气动装置具有较长的使用寿命,并有助于降低长期运营成本。就油、水或灰尘颗粒而言,低于或不符合压缩空气质量标准将对气动组件的使用寿命产生负面影响,从而导致能源和运营成本增加。Festo 节能服务提供的气源质量分析可以测量残留油含量和压力露点,发现其中的不足之处并提出改进建议,例如,建议客户增加过滤器的更换频率。经过优化的维护措施平均可节省 35% 的成本。

节约压缩空气

理想情况下,应从压缩空气的源头(即压缩机)开始采取节约措施。通过分析制备压缩空气所消耗的电量(在 24 小时内进行),可以得到详细的电力和压缩空气消耗量曲线以及压力水平数据。在最合适的时间段运行压缩机有助于优化其利用率。实施灵活的操作方案可在不需要压缩机时将其关闭,这有助于十分有效地分配电力资源, 从而可以确保可用压缩机容量的利用率达到最佳。在待机状态下使用机器测量压缩空气的输送速度,可以了解泄漏损失的具体数值,从而在整个压缩空气系统中节省成本。

因此,对于公司来说,在系统运行时进行准确的分析,以便识别压缩空气系统中缓慢的能量损失,这一做法是非常值得的。一旦将分析结果转化为优化措施,就可以节约每天的宝贵能源。Festo 节能服务专家经验丰富,他们知道应该从何处入手寻找系统弱点。他们精湛的分析技能和改进建议可以帮助公司节约每天的成本。