Remote I/O, or RIO, short for remote input/output, is a system with which various sensors and actuators can be connected at decentralised locations within a plant or network and their data can be managed via a central controller. Nowadays, remote I/O is an essential part of modern automation solutions, as it supports the flexible integration and scalable expansion of automation networks. This is particularly important in complex industrial environments in order to efficiently manage all the necessary processes. By integrating remote I/O, industrial control systems can be changed and extended more flexibly without the need to make major changes to infrastructure. By using remote I/O, companies can reduce their operating costs, increase efficiency and simplify maintenance. Close cooperation with central control units and communication protocols such as PROFINET, EtherCAT® or Ethernet/IP is crucial for reliable data transfer and system performance.
A local or central I/O is installed in the control cabinet together with the PLC. A remote I/O, on the other hand, is decentralised and installed separately from the control unit.
The choice between deciding on a local I/O or remote I/O depends heavily on the individual requirements and framework conditions of an application, e.g. a centralised architecture may make sense in smaller systems, while larger, more complex networks may benefit from the strong points of a decentralised structure. Another aspect that companies should consider is compatibility and integration with existing controller systems to guarantee seamless and efficient implementation.
Decentralised I/O is a remote I/O system with a predefined number of inputs and outputs. It is a self-contained unit and cannot be expanded.
Watch our animation to see how modern architectures make your automation simpler, faster and more cost-efficient.
Remote I/O is used in a wide range of industrial and process automation systems to reduce the amount of wiring required. In the chemical and pharmaceutical industries, remote I/O systems enable production processes to be precisely monitored, thus contributing to compliance with strict safety and quality standards. Remote I/O is used in the energy and utilities industry for operating power stations, water treatment plants and distribution networks. It is also used in the automotive industry in larger applications such as production lines and robot cells. Ultimately, the possible applications of remote I/O are as diverse as the requirements of the various industries, which only further emphasises its importance for modern automation solutions.