Two ways to control nitrogen: simple or intelligent

1: Fixed orifice or adjusted throttle valve – cheap, simple, but with limitations

Orifices are the simplest form of nitrogen flow control. These are mechanical tapers (fixed drilled holes) in the tubing system through which a specific amount of nitrogen flows at constant pressure. The advantage: extremely favourable total costs, often less than €90  including installation as well as a simple switching valve and the orifice itself. This makes them ideal for adjusting simple flow rate applications for nitrogen with stable conditions.

A frequently used product in this context is the MH1 valve. This is an inexpensive standard valve which, in combination with an orifice, offers a functional, analogue solution for regulating the gas flow rate in industry. In many applications, this combination is sufficient, especially if the investment pressure is high or no digital feedback is required.

However, there are clear limits:

  • Hardly any flexibility: changes in nitrogen requirements are difficult to map.
  • No reaction to pressure fluctuations: if the input pressure drops, the flow rate drops too and go unnoticed.
  • No monitoring: it is not possible to monitor the flow or to gather data

Please note: if you still want to record measured values at a later date, additional hardware is required (e.g. separate pressure or flow sensors and the necessary input on the controller), which increases the costs and system complexity. Despite the very long service life and reliability of simple switching valves such as the MH1, they are not ideal for processes in which cleanliness is critical. Their design means that higher particle emissions are to be expected compared to dedicated mass flow controllers.

However, many production lines continue to rely on this principle, especially when only simple volumetric flow rates need to be kept constant and appropriate filters reabsorb the particles. But as soon as dynamic adjustments, reliable monitoring or process traceability are required, this solution quickly reaches its limits.

2: Intelligent regulators – precise, data-capable and future-proof

Mass flow controllers such as VEFC, VEMD or VEAD offer methods for regulating the nitrogen flow rate that fixed orifices or adjustable throttle valves cannot.

  • Dynamic control of the nitrogen flow
    Even when the input pressure fluctuates, the required volumetric flow rate remains constant. This protects sensitive processes.
  • Process reliability through monitoring
    These products provide real-time feedback, for example whether the flow rate is within the required range. If the pressure drops, a warning can even be issued automatically.
  • Use in complex systems
    The data can be read out centrally via controllers and used for cost centre accounting or process optimisation, for example. This is particularly interesting if nitrogen is provided and billed internally based on consumption.
  • Prerequisite for predictive maintenance & AI
    Regulators continuously supply data (e.g. flow rate, temperature or pressure, if applicable). That can then be integrated into platforms such as Festo AX to monitor the nitrogen flow rate for predictive maintenance and data analyses.

The products themselves are not "intelligent" in that they can autonomously detect anomalies but they are AI-ready. In conjunction with filter monitoring, pressure sensors and algorithms, the degree of pollution of filters can be detected, for example, which enables timely servicing without interrupting production.

What are the different type of valves and what are they suitable for?

Before deciding on a specific valve, you should take a close look at the technical requirements and the application environment. Each valve has its own strengths, be it in terms of flow rate, size or connectivity.

为什么有时价格高昂的产品反而性价比更高?

虽然简单系统的购置成本更低,但搭载监控功能的可靠减压阀却具有决定性优势:

  • 过程可靠性:输入压力波动不会导致流量变化
  • 实时反馈:实现预测性维护的明智选择;可实现内部消耗测量
  • 可扩展性:尤其在控制点较多的复杂线路中,可立即识别到异常
  • 总体拥有成本:精确的系统可将流量精准控制在所需程度,从而达到主动节省氮气,最终降低电耗和减少 CO2 排放量的目的。

示例:在装有 50 个减压阀的装置中,每台设备上的简易显示屏可以帮助用户快速识别缺陷区域,而无需逐一读取数值。

前景:整装待发,支持人工智能和预测性维护

先进的质量流量控制器可以提供宝贵的数据,比如流量、压力、温度等,这些数据可以集成到 Festo AX 等上级系统中。 这使以下功能成为可能:

  • 成本中心测定消耗量
  • 通过压差监测过滤器磨损情况
  • 基于真实负载数据进行维护预测

这些设备本身并不“智能”,但它们支持 AI,也为面向未来的数据支持型制造工艺奠定了基础。

决策支持:适合您工艺的正确解决方案

选择阀时,需要考虑多种因素:

  • 所需流量范围
  • 能源消耗
  • 工艺要求(比如:  洁净室等级)
  • 能否集成到现有控制器中
  • 监测和读数需求

未来我们将使用互动工具进行个性化推荐,从简单的节流孔到支持 AI 的 VEFC,通过有针对性地询问为您推荐最合适的解决方案。

结论

半导体制造中的氮气调节远不止是技术小问题这么简单,它对质量、工艺稳定性和成本都有影响。 无论简单解决方案还是高度先进的闭环控制技术,决定性因素都是您的应用需求。 做出正确的选择,不仅能确保安全运行,还可提高效率和未来竞争力。