“In fact, we’ve actually created a very small factory", explains Niels Kruize, responsible for business development at Synchron Lab Automation. “Recently, one of our customers made a priceless statement. He said, “This is so beautiful and at the same time so simple, I just don’t understand why it hasn’t been invented before.”

The process running on the machine is used in the agricultural industry for plant breeding. The DNA is extracted from shredded plant material. Components from Festo carry out important functions in all extraction phases. The process begins with a holder which accommodates up to 400 microwell plates – 200 for input and 200 for output.

Festo’s Bert Baas adds: “It’s a perfect example of a combination of industrial and laboratory automation.” The machine’s hardware is subdivided into functions, each of which is designed as simply and efficiently as possible. The small factory is equipped with serial instead of parallel drives. Plates are continuously moved and positioned throughout the pipetting, rinsing and washing stations.

Right from the start, the developers at Synchron received intensive support from Festo. Key Account Manager Bert Baas from Festo explains: “Our automation experts provided support throughout the entire development of the extraction machine. For example, they suggested using the new CPX-E unit to provide genuine added value. They used the unit in this project before it was even available on the market.”

How the DNA extraction machine works

The extraction machine runs continuously for eight hours and can also be operated 24 hours a day without any problems in case of increased demand. Its capacity is already eight times greater than other options currently available on the market.

Identification and transport:

The bar code reader SBSI scans all the microwell plates at the start of a run. Electric axes EGC, in combination with a semi-rotary drive DRRD and a gripper DHPS, pick up the microwell plates and place them on carriers which move through the various stations on a transport system.

Rinsing:

Metal micro-spheres are added to separate the DNA from the other material. The DNA attaches itself to the micro-spheres, while the rest of the material floats up in the microwell plates. Liquid is added to and extracted from the microwell plates at several washing stations. The pipetting head is lowered by an electric slide EGSC during this process. After rinsing, clean DNA remains in the microwell plate and is fed to the final processing step, namely DNA extraction, via the transport system.

提取:

电缸 EGC 与滑台电缸 EGSL 一起控制抓取用于提取 DNA 的移液头。每块板有 96 个样品。提取过程总共需要 20 分钟。每 2.5 分钟开始一块新板。

该机器具有串联和模块化结构,运行时几乎完全没有任何切换延迟。CPX-E 和带有 IO-Link® 的阀岛 VTUG 用于控制系统。CPX-E 被开发为带有 EtherCAT 主控制器和运动控制器的远程 I/O 系统或 PLC,以确保控制单元与电驱动器的简单组合。

超越极限 — 合营企业

Synchron Lab Automation 的所有者兼董事总经理 Derk Wilten 解释了与 Festo 的合作是如何实现的:“过去,我们只专注于解决方案概念,后来获得了创造解决方案的合作伙伴。这是因为我们最初是一家软件公司。当 Niels Kruize 加入公司时,他建议我们应该自己开发交钥匙解决方案。他对此深信不疑。Niels Kruize 负责 Synchron Lab Automation 的业务开发。他曾在英格兰工作,在那与 Festo 密切合作过。根据他的积极经验,他建议推出第一款具有 Festo 工程知识和组件的“内部设计产品”。

信任该项目的合作伙伴

Niels Kruize 解释说:“Festo 是一家领先的公司,拥有全球零部件供应商网络和全球服务与支持。Festo 的专家帮助我们进行设计,并与我们分享知识。他们了解不同的市场并知道如何运营,这非常有价值。Synchron 为世界各地的客户提供服务。因此,对于在德国交付零件的速度与在新加坡一样的合作伙伴,我们很高兴与之合作。” Derk Wilton 很快就赢得了胜利:“Festo 使用的运营方法与我们完全相同。与信任该项目的合作伙伴合作令人非常放心。”

Niels Kruize 很高兴他对合作伙伴关系的信心得到了确认。"它为我们提供了巨大的附加值。合作伙伴关系是双方真正的合作。这个项目对两家公司来说都是全新的任务 — 通信技术对我们来说也是全新的领域。我们彼此学习,着眼未来,期待下一步。" Bert Baas:“我们与 Synchron 讨论新技术,并预想它们提供的可能性。这为 Festo 提供了新的动力。”

关于 Synchron Lab Automation

自 1985 年以来,Synchron 一直在开发用于实验室自动化的解决方案,并且专门从事液体、管和板的自动化抓取。近年来,Synchron 在其产品组合中增加了针对农业生物行业的创新设计和专用自动化平台的构建。其中包括采种、发芽、种子健康测试和 DNA 清洁系统。Synchron 的 Experimate™ 软件平台提供了用户友好的界面,并控制了 Synchron 的所有系统和连接模块 — 从 LIMS 连接到自动化工作场所。

www.synchronlab.com