Compressed air is used in a wide range of industries – from food and beverage to pharmaceuticals, electronics, and automotive manufacturing. Contaminants such as water vapor, oil, and particulates can compromise product quality, damage equipment, and even pose safety risks. Poor air quality can lead to unplanned downtime, increased maintenance costs, and product recalls in regulated industries.
For example, in a food processing plant, oil or moisture in the air line can contaminate packaging or ingredients, leading to health risks and regulatory violations. This example highlights the importance of tailoring air preparation to the specific needs of each application.
Additional Considerations:
The international standard ISO 8573 provides a comprehensive framework for measuring and classifying compressed air contaminants. It breaks down air quality into three main categories:
Each category is assigned a class rating, with Class 1 being the highest quality. For example, ISO 8573-1:2010 is the most commonly referenced part of the standard, specifying the purity classes for compressed air. A typical classification might look like ISO 8573-1:2010 [1:2:1], meaning
Different industries have unique requirements for compressed air quality:
Festo collaborated with TNO at the Van Leeuwenhoek Laboratory to enhance compressed air quality and capacity. Following a pre-audit, Festo and Royal HaskoningDHV designed a two-tier system meeting ISO 8573—delivering extremely dry compressed air (Class 2.1.1) for sensitive tests and standard-quality air (Class 2.4.1) for other uses. The result: higher reliability, better efficiency, and optimized energy consumption.
To meet the desired ISO 8573 class, various air treatment technologies are used in combination. These technologies are typically arranged in stages to progressively remove contaminants.
Water is one of the most common and damaging contaminants in compressed air. It can cause corrosion, damage pneumatic tools, and affect product quality. Key technologies include:
Solid particles can originate from ambient air, the compressor, or the piping system. To remove them:
Oil contamination can come from lubricated compressors or ambient sources. Removal methods include:
Collected water and oil must be safely discharged:
Even with the best intentions, many factories and maintenance engineers make avoidable mistakes when designing or maintaining their air preparation systems:
Avoiding these pitfalls starts with a proper system assessment and regular monitoring of air quality.
ISO 8573 is an international standard that defines the quality classes for compressed air based on the concentration of contaminants such as particles, water, and oil. It is important because it helps industries ensure their compressed air meets safety, efficiency, and product quality requirements.
The required ISO 8573 class depends on your industry and specific application needs. For example, pharmaceutical and semiconductor industries often need Class 1 air (ultra-clean), while automotive paint booths may require Class 2. Assessing the sensitivity of your process and consulting industry guidelines will help determine the correct class.
The standard addresses three main contaminant categories: particulate matter (dust, rust), water (vapor, liquid droplets), and oil (liquid oil, aerosols, vapor).
Common technologies include cyclone water separators, refrigeration and desiccant dryers, particulate pre-filters and high-efficiency filters, coalescing and activated carbon filters for oil removal, and condensate drains and oil/water separators for condensate management.
Regular testing frequency depends on the criticality of the application but typically ranges from quarterly to annually. High-risk industries or processes may require more frequent testing to ensure ongoing compliance.
Poor air quality can cause equipment damage, product contamination, increased downtime, higher maintenance costs, and safety hazards. In regulated industries, it can also lead to non-compliance and costly recalls.
Oil-free compressors significantly reduce oil contamination risk but may not eliminate it entirely due to ambient contamination or piping. A comprehensive air treatment system is still recommended for critical applications.
Regular replacement of filters and desiccants, cleaning or replacing condensate drains, monitoring pressure drops, and scheduling periodic air quality testing are essential maintenance practices.
Avoid undersizing equipment, ensure proper placement of air treatment components close to the point of use, perform regular maintenance, and consider ambient conditions such as humidity and dust when designing your system.
Yes, integration of IoT-enabled sensors for real-time air quality monitoring, predictive maintenance using data analytics, and increasing adoption of energy-efficient and environmentally friendly air treatment technologies are key trends.