Drawing circles in the sky. From left to right. Up and down. Completely weightless. As free as a bird. What young and old often dream of can become reality in Burgenland, Austria. A breezy flight at 22 meters (72 feet) above the ground on “Leonardo’s Flying Machine” is just one of many attractions at Familypark in St. Margarethen that makes children’s eyes light up and is lots of fun for the whole family. And the technicians at the amusement park also had fun during an in-house training seminar held by Festo Training and Consulting directly on-site in St. Margarethen. For two days, everything revolved around the topics of pneumatics and electropneumatics – and only marginally on merry-go-rounds. And there are plenty of those at Familypark not far from Lake Neusiedl. Austria’s largest amusement park has around 60 smaller and larger attractions spread over an area of 145,000 square meters (approx. 36 acres).

Adventurous diversity

From the nostalgic steam locomotive tour through the woods and meadows, to the spectacular roller coaster ride, the park thrives on its diversity. There is good reason why, in addition to four underwater parks, there is a concert hall, restaurants, and climbing gardens that are open from mid-March to the end of October. The 633,000 visitors who experienced the Burgenland adventure world in 2016 are testimony to an increasing yearly trend. In 2018, the family business celebrates its 50th anniversary – all well equipped. Or rather, well trained.

A special pneumatic setting

Together with a specialist from Festo Training and Consulting, several park employees took a ride on the “valves roller coaster”. Two days without any dizziness or fear of heights. Long-time Festo Trainer Nobert Berneck made sure of that: “The seminar was especially exciting for me too. Pneumatics is used here in somewhat unusual settings, ranging from animated figures to large systems.”
Even the basic knowledge of the participants – a group of electricians, machine technicians and mechanics – was very different. This made it all the more important to adapt the content of the course to the needs of the park employees.

安全方面

一个需要特别注意的主题:正确的维护。“对我们而言,客人的安全始终是头等大事。这意味着所有设备始终处于最佳维护状态,我们必须立即对任何可能的故障做出响应,” 家庭公园运营经理 Michael Lichtenberger 说道。“我们的大多数景点都配备了气动元件,例如气缸和阀,应用范围从过山车制动器到入口的安全门。因此我们的培训能给我们带来最新的只是。” 气动回路如何工作?制备压缩空气的最佳方法是什么?户外景点可能会发生什么样的危害?我们如何进行控制,以增加或减少速度?这些都是核心问题。“对我们来说,尽可能提高员工的意识非常重要,例如效率问题以及压缩空气消失后所产生的成本,” Lichtenberger 解释道。

多练习,多关注

正如参与者的态度所表明的那样,研讨会的内容当然不会消失。“尽管我们的员工来自许多不同的领域,但研讨会对每个人都极具启发性。这要归功于 Festo 的高素质培训师,”家庭公园技术总监 Erik Kovács 说道,他首先赞扬了大量的动手实践经验:“理论部分通常会在一段时间后被遗忘,但是实际看到并亲自尝试的内容不会淡忘。” 负责工作和操作安全的初级经理 Dominik Müller 也有相同的看法:“主题准备得很好。这很重要,因为我们非常重视景点和顾客的安全。” 然后他继续笑着说:“你从学校就知道这一点。大多数人在上理论课时都昏昏欲睡,但是一旦有体验活动,每个人又精神得不得了。在我们的研讨会上,理论与实践完美结合 — 没有人会睡着。”

以个性化达到新高度

正如每个公园景点都很特别一样,该课程也根据参与者的个人需求进行了匹配。“我们感兴趣的事物是以令人兴奋的方式介绍给团队的,”运营经理 Michael Lichtenberger 以积极的口吻总结道。“我们明确了所需的知识种类,而这些正是 Festo 提供的内容 — 完全符合我们的要求。” 而且,他很高兴与他的员工又迈出了一步,以最大程度地减少停机风险,并进一步提高操作安全性。
因此,没有什么能阻止乐园为所有家庭带去的绝对乐趣,并在未来飙升到新的高度。例如,莱昂纳多·达·芬奇飞行器上的这句话:“体验飞行之后,回到地面,您将举目望向曾触及过的天空,渴望再来一次 。”

  1. 本文发表在 Festo Didactic 的客户杂志《资格发展趋势》第 1.2017 期上
  2. 图片:Familypark / Festo / Hollunder / Matula / Draper