1. Why is it important to optimise the pressure or flow rate?

Ulrich Sixt: For automation to be efficient, both variables need to be precisely controlled. In pneumatic systems, pressure and flow rate are inextricably linked. A cylinder does not only move because there is pressure,air must also flow to enable movement. That means purely static pressure control is not sufficient.

A well-coordinated closed-loop control system has several advantages. Energy efficiency plays a big role, as an excessive compressed air supply leads to unnecessary consumption and rising costs. Proportional-pressure regulators can help to precisely control the air flow and supply only the required amount. Last but not least, when using precise closed-loop control, sudden pressure fluctuations are avoided and the service life of the components is increased, as fluctuations accelerate the wear of valves and actuators.

eBook: Controlled Pneumatics made simple ​

How to make your pneumatics digital, efficient and highly precise.​

Discover how Controlled Pneumatics opens up entirely new areas of application for regulating pressure, flow, and motion. Find out how proportional technology, sensors, and intelligent algorithms work together in a closed control loop to improve your processes. Gain valuable insights into how you can quickly and easily make your pneumatic systems more efficient, cost-effective, and powerful.​

Download now!

2. What are the developments in pressure or flow control, and how do they differ from conventional systems?

Ulrich Sixt: Proportional technology, sensors and intelligent algorithms in modern automated systems significantly optimise precision and efficiency. One of these developments are regulators that are pneumatically or electrically controlled. These adjust the flow rate and pressure to a setpoint value or to an external signal, which is interesting if the process requires different pressures. Proportional pressure regulators keep the system pressure constant in real time, regardless of fluctuations.

In many applications, pressure and flow rate are still controlled manually or with simple regulators. These are tried and tested, but often insufficient for greater precision and efficiency. Manual valves, for example, require regular readjustments as they do not adjust automatically to pressure fluctuations.

3. What advantages do modern proportional pneumatic valves offer for automation?

Ulrich Sixt: The pressure, flow rate and movement can be very accurately controlled thanks to the intelligent combination of highly dynamic final control elements, sensors and control algorithms. Everything is automated, efficient and adaptable to a wide range of process requirements. It is precisely this principle that Festo has successfully implemented with Controlled Pneumatics.

Modern proportional pneumatic valves operate in a dynamic, closed control loop, facilitating continuous adaptation to changing conditions. Sensors continuously measure the current pressure and transmit the values to the electronic control systems. This compares the measured actual value with the specified setpoint value and immediately identifies deviations. The valve reacts in real time and automatically increases or reduces the pressure to precisely maintain the required value (flow control). Flow regulators play a crucial role in this control loop. They ensure that the volumetric flow rate is precisely dispensed to optimise energy consumption and at the same time guarantee constant performance. This intelligent closed-loop control system makes for stable process conditions, reduces energy losses and increases the efficiency of the entire system.

4. What are the advantages of intelligent pressure or flow control?

Ulrich Sixt: Intelligent pressure and flow control increases efficiency, process stability and plant and system availability. Precise closed-loop control without fluctuations optimises energy consumption and improves product quality. Constant pressure protects pneumatic components from excessive stress and wear. This increases process reliability. The automated adjustment also means that different materials and processes can be flexibly controlled. This reduces operating costs without compromising performance.

5. 智能压力控制或节流技术是何种方式来提高过程安全性和保证质量?

Ulrich Sixt: 在实际应用中,我屡次接触到因压力或流量波动而导致产品缺陷的案例。 特别是在汽车工业、医疗技术、食品和包装等敏感领域,稳定的过程对于避免产生废品和返工至关重要。

有一个常见的问题是, 不同生产工位的压力不同,因此可能会导致气缸未准确定位部件,或向密封件施加的力不正确。 在这种情况下,具有闭环控制功能的比例阀便可大显身手。 无论负载如何变化、入口压力如何波动或出现泄漏,这类阀都能将压力保持在所需水平。 在实际应用中,这意味着, 过程波动可能会导致废品率升高,而智能控制装置可显著降低这一概率。

我的结论是, 如果想提高过程安全性和质量,那么精确、自动化的压力或流量控制必不可少。 借助这种控制装置,不仅能减少故障,还能确保产品质量的一致性,缩减停机时间,提高装置整体效率。

按需网络研讨会: 工作中的受控气动系统

在本场网络研讨会中,我们将通过真实案例展示受控气动系统如何精确调节压力,并实时对作用于组件的扰动变量进行补偿。 全面了解该技术,知晓其与标准阀的区别,以及其如何为您的应用场景带来可量化的增益。

观看网络研讨会

6. 您认为压缩空气的生产在能源效率方面有哪些潜力?

Ulrich Sixt: 压缩空气是工业领域最昂贵的能源之一,因为压缩机生产压缩空气需要消耗大量电力。 然而,许多系统的运行压力高于所需的压力,导致产生了不必要的能源消耗。 即使仅将系统压力降低 1 bar,也能显著降低能耗。

而智能化的压力控制或节流装置便可确保仅提供实际所需的压缩空气。 传统系统通常以最大系统压力运行,而带传感器反馈机制的现代比例阀可根据实际需求动态调整压力。 由此最大限度减少了泄漏损耗,在许多企业,泄漏损耗高达压缩空气消耗量的 20 %。 此外,基于需求的控制系统还可优化压缩机的使用,缩短压缩机运行时间。 这些优势直接体现为能源成本的降低。 在大型装置中,每年由此可节省数万欧元。 如果采用智能减压阀和流量调节阀,企业不仅能降低能耗,还能同时提高可持续性和运营效率。

7. 数字化在压力控制或节流中发挥着何种作用?

Ulrich Sixt: 数字系统的核心优势,是数据的透明化和可用性。 借助数字系统,可通过 IO-Link® 或其他现场总线的接口随时调用压力或流量值,并有针对性地进行优化。 通过这种方式,企业就能及早发现压力损耗或泄漏,避免导致故障。 在实际应用中,我们发现,企业实现系统互联后可大大缩减计划外停机时间。

此外,也能更加灵活地调整相关过程。 在现代化生产线中,压力或流量值可根据材料或产品自动调节,无需技术人员现场手动干预。

简而言之, 数字化减压阀或流量调节阀可提高过程安全性、降低维护成本,实现面向未来的灵活生产。 企业实现系统互联后,可提高整个生产过程的效率、透明度和控制度。

8. 压力控制或节流技术的发展方向是什么?

Ulrich Sixt: 我认为,压力控制或节流技术的进一步发展主要面临着三大核心要求:提高精度、能效以及数字化水平。 通过将传感器直接集成到控制阀中,可使测量和闭环控制技术合二为一。 这样可以节省空间,简化安装过程,提高反应时间。

半导体生产或医疗技术等敏感行业依赖于先进的阀门技术。 例如,压电或动圈技术可以实现更快、更精确和更高效的控制。 第三个发展方向则是借助人工智能实现自适应压力控制或节流。 未来,基于人工智能的算法可自动优化过程,使其适应不断变化的生产要求。

9. 对于希望提升自身压力控制或节流能力的企业,您有何建议?

Ulrich Sixt: 如果您想在生产中提高效率、过程稳定性并且节约能源,那么我建议关注智能控制方案。 Festo 开发的受控气动技术就是一种将比例技术、传感器技术和数字控制相结合的解决方案,可精确、节能、灵活地控制压力和流量。

与固定设置的传统系统相比,受控气动系统可实时动态调整数值。 由此不仅可提高生产质量,减少空气消耗量,还能延长组件的使用寿命。 若您希望深入了解该技术,请翻阅我们的电子书,查看智能压力控制或节流技术如何实现降本增效——既降低运营成本、稳定过程,更能助力企业从容应对未来挑战。

10. 预测性维护在压力控制或节流中发挥着何种作用,有哪些优势?

Ulrich Sixt: 对于实现稳定、高效的压力控制或节流,预测性维护起着决定性作用。 由于传感器会持续测量压力、流量和温度,因此即使是最微小的偏差也能及早发现。 这样一来,就能及早识别出磨损或潜在故障,并采取相应措施进行预防。 我们在必要时介入干预,而非死板地遵照维护周期——这一策略可减少意外停机与维护成本,同时显著延长组件使用寿命。

当然,将这些系统集成到现有装置中也是一大难题,尤其是在数据处理和分析方面。 但随着现代数字化解决方案的发展,预测性维护正日益成为标准方案。 这种方案有力地促进了自动化效率、可持续性和过程安全性的提高。

感谢 Ulrich Sixt 就压力控制或节流相关问题提供的真知灼见。 根据他的专业意见,智能技术不仅能稳定过程,还能节约能源和提高生产质量。 采用数字比例阀与互联控制技术的企业,能够实现效率提升、预测性维护和极高的灵活性——这标志着气动技术正迈向前所未有的智能时代。