The solution from Festo is part of a modular JANUS® G3 liquid handling workstation that is flexible and can be adapted to various customer requirements. The following process steps are considered in the application: Separating the different sizes of vials from the rack → Identifying the samples → Vortexing → Opening the cap → Placing the opened sample under a pipette → Closing the cap after sampling → Placing the vials back in the rack.
Two different types of vials with very different dimensions need to be handled: ThinPrep®: 42 mm diameter x 75 mm height and SurePath®: 33 mm diameter x 52 mm height.
The caps of the vials are flat and therefore not ideal for automation. This places special demands on opening and closing with a high torque value of up to 2 Nm. Because of the special geometry of the bottom of the vial, even the slightest change in position can make it impossible to place the vials back into the rack.
The customer wanted a fully electric industrial robot that covers a working area with 2 trays of 48 sample vials each. The solution also had to perfectly match the overall system visually without requiring modifications to the existing platform. In addition, an option to retrofit systems already on the market was also a requirement.
Festo developed a total of five subsystems consisting of Festo standard components, a PerkinElmer® JANUS® G3 workstation and a customised rotary gripper module.
通过与客户紧密合作,Festo 最大程度降低了该工业机器人的复杂性。该工业机器人(三维门架)使用 JANUS® G3 工作站中现有的导轨,因此可以选择紧凑型轴。带有经过改良的标准抓手的旋转抓取模块是该三维门架的一部分,用于从托盘中取出单个样本容器。条形码阅读器明确识别样本容被后,会绕垂直轴快速旋转,以确保样本容器中的样本与悬浮液混合。然后就会打开样本容器,并将其放在移液管下。取样后,容器会再次合盖并放回托盘中。
在所有过程步骤中,样本容器的盖子始终都由旋转抓取模块夹持。这样就确保每个样本容器在打开和关闭后都能非常精确地放回托盘中。
整个工作站的几个 Beta 版本目前正在由选定的最终客户进行测试。同时,整个系统将经由 TÜV 认证,以便未来销往更广阔的市场。
通过与 Festo 合作,客户获得了诸多助力。Festo 的样本运送解决方案提高了整个系统的速度、灵活性和过程安全性,最大限度地降低了复杂性、提高了组件使用效率。此外,客户还能降低开发成本,缩短产品上市时间。未来,客户将进一步加强与 Festo 的协作工程合作,因为由此客户可以专注于战略创新,并对不断变化的市场要求更灵活地作出反应。
仅供研究使用。不用于诊断程序。