Simplicity

Pressure-controlled dosing systems are mechanically simple and only require a small number of components A pressure regulator, together with a safety valve, pressurises the tank containing the liquid. The pressure then pushes the liquid through the tubing and the solenoid valve. Next, the nozzle releases the liquid into the vial via a needle tip with a specific opening. Thanks to an easily integrated pressure vacuum generator, it can be operated anywhere, even in laboratories without a central compressed air supply. The system has few moving parts and is easy to clean, maintain, and parameterise. The pressure is set depending on the medium and the opening time of the valve can be adjusted for the required volume. The basic design is always the same, but different valves can be used depending on the liquid. Media-separated liquid valves, which must be resistant to chemicals when dealing with aggressive media, take care of dispensing, while gas valves are used for pipetting. Aspiration is carried out via a vacuum. Disposable pipette tips prevent contamination when using different liquids. A graphical user interface (GUI) is used as the operator environment.

Precision

Handling minute volumes of liquids is a hugely important step for a large number of processes in laboratory automation. With pressure-controlled dosing systems, volumes from 1 μl can be dispensed precisely and reliably with a coefficient of variation of < 1% (depending on liquid volume and ambient conditions). The speed of the liquid can be uniquely controlled via the pressure, and independently of the dispensing, aspirating, and pipetting functions. Users can precisely adjust the system for optimal flow and precision, so a clean drop break-off can be achieved for reproducible accuracy. Solutions with sensitive liquids such as suspensions can be handled more gently using lower pressures. In addition, there are many different options for monitoring the process.

Flexibility

Pressure-controlled dosing systems are open and flexible. Many parameters can be changed and individually adjusted, enabling a wide range of different liquids to be precisely dispensed. The systems can also be individually extended or adapted to specific needs.

Scalability

Since many laboratory processes require liquids to be handled precisely, automation leads to significant productivity gains and improved process reproducibility. One of the biggest benefits of pressure-controlled dosing systems is their scalability. For example, individual dispense heads can be combined by mounting them on a rail with a freely selectable grid. All dispense heads can be controlled independently to dispense different liquids simultaneously or to set different volumes.

生产力

如需提高生产率,用户可以将滴定头集成到平面门架上。该子系统可以在紧凑的工作空间内实现运动学移动以及运送液体,例如准备样本或向微孔板添加液体。压控式分配系统能够实现很高的通量。与其他系统相比,高流速和恒定的流体压强提升了其性能。

Festo 开发了全面的压控式分配系统产品组合,这些产品的扩展和组合也非常方便。欢迎联系生命科学领域的 Festo 专家,共同探讨哪些解决方案最能满足您在精确度、灵活性或通量方面的要求。