Autonomous pressure and vacuum generation

When designing devices for liquids operated by compressed air, external compressed air sources must always be taken into account, as liquid handling systems usually require a constant air supply. The most common supply is via a wall connection; however, this restricts the flexibility of the system. And having to retrofit air ducts would lead to higher costs.

That is why Festo has developed a module for generating pressure and vacuum that does away with the need for compressed air supply via supply lines. This compact submodule is an integral part of the liquid handling system. The generator builds up a specific pressure and vacuum. If the values fall below a specific threshold value, the supply is activated and the pressure and vacuum built up again. This is done using various sensors, a pump and a distributor.

Multiple dosing with reservoir and scale

Festo designed a special manifold duct plate with a reservoir for the dispense head VTOE for multiple dosing with maximum repetition accuracy. This makes it possible to draw in up to 2 ml of liquid. The dispense head works in conjunction with a scale positioned under the microwell plate, thus creating a closed feedback circuit for the dosing process. By having continuous feedback, the opening time of the pneumatic valve can be fine-tuned to achieve accurate dosing volumes.

After drawing in the required volume for the total dosage, the liquid is dispensed into each well in three injection phases. During the first and longest phase, most of the liquid is dispensed. The second injection phase is shorter and gets closer to the required volume. The last injection is very short in order to achieve the exact filling quantity. Exact means that accuracies better than 1% CV can be achieved.

Easy to adjust and operate

This solution includes a graphical user interface (GUI). It enables laboratories to carry out tests to meet individual requirements without having to reset the system every time. For example, the GUI allows the user to select from which vial to aspirate, how much fluid is dispensed into each well of a microwell plate, and how many wells are to be filled in a particular row. While the liquid is being dispensed, the GUI provides a live display of the scale to indicate the amount of liquid dispensed. The amount of liquid is used to calculate the average mass and the coefficient of variation (CV) of the dosage.

The GUI gives the user access to additional functions such as rinsing the liquid in the manifold duct plate until only air is left, or cleaning the manifold duct plate by drawing in and rinsing using a cleaning solution.

动态体验创新型液体搬运系统

本文介绍的系统是 Festo TEC Boston、Festo LifeTech 北美开发中心和Festo 德国总部紧密合作的成果。在视频中,您可以看到所有子模块的运行情况。为了实现快速、精确的运动,系统采用了遵照平行运动学驱动理念的紧凑型 EXCM 平面门架。

展望未来

TEC Boston 的团队已经在规划下一步的开发目标:一个可以根据即插即用原则进行安装的压力和真空产生模块,它可大大缩短安装时间。