Heiko Fleischhacker: Energy efficiency is crucial for the competitiveness and sustainability of any company. However, when looking at compressed air systems, I always notice that the focus is often only on power consumption. Many companies already focus on energy-efficient lighting or photovoltaics, but the potential in a compressed air system is often overlooked.
When looking at energy efficiency in compressed air, they usually only consider the compressors. Discussions about high costs often centre on compressed air generation. However, the entire compressed air system, from generation to the use of the compressed air, must be analysed. Having a partial view means that valuable savings potential goes unrealised.
Heiko Fleischhacker: Producing, distributing and processing compressed air energy efficiently is complex. Although many customers are specialists in their own production processes, they have only limited knowledge of the compressed air systems used in their plants. In my experience as an auditor, many customers don't know which adjustments they need to make in which order to achieve a long-term increase in efficiency. Energy management and maintenance staff often lack the necessary expertise in pneumatics. Optimising compressed air is more than just eliminating leakages. It requires broad technological expertise and a thorough understanding of the compressed air system, from the compressor station to the pneumatic application. For example, a few weeks ago I carried out an audit at an established pharmaceutical company. The compressed air they produced was of a very high quality. But they never asked themselves if this was actually necessary for the production process. By making a small adjustment to the compressed air quality, we succeeded in making lasting energy savings extremely quickly. This shows once again how important it is to have a complete overview of the compressed air system, the compressed air requirements and an in-depth understanding of pneumatics.
Heiko Fleischhacker:压缩空气能效审计是对企业的压缩空气系统进行整体评估——从压缩机房到气动应用都在审计范围内。目的是找出效率低下的领域并确定节能方案。这样不但能降低成本,还能减少碳排放,进而提高生产率、推动可持续发展。通过审计,企业有机会能够了解压缩空气系统的多个关键领域,还能得到相应的解决方案。审计通过透明的方式,披露压缩空气的生成效率、自有压缩机的利用率,以及压缩空气穿过系统的效率情况。据此可以确定基础设施的改善潜力。
此外,审计还能提供压缩空气质量相关的重要信息。在满足生产需求和保证可靠的机器性能方面,这些信息至关重要。审计还会披露压缩空气在不同应用中的使用效率。企业最终会收到一份包含精确数据和优先行动建议的详细报告,可以据此优化整套压缩空气系统。这份囊括所有测量结果在内的最终报告,可用于符合 ISO 50001 标准的能源管理。
Heiko Fleischhacker:对于那些希望优化压缩空气设备的企业,我总是建议采取结构化方案。由于不同组件之间直接关联运行,因此对压缩空气系统进行整体评估至关重要。在某个位置(点)做出改变,总会对整套系统的性能和效率产生影响。一旦发生泄漏,或者出现压缩空气处理不当等情况,设计再优良的压缩机站点也会丧失其在能效方面的优势。
简单来说,只有着眼全局,才能成功掌控压缩空气系统的能源效率。安排一次压缩空气能效审计,不但能打下必要的信息基础, 还能收到一份关于优化措施正确实行顺序的明确行动建议。后者与前者同样重要。
Heiko Fleischhacker:如果企业希望对压缩空气设备进行客观评估,精确了解设备的当前状态,那么不论何时审计,都有意义。我建议企业针对 DIN ISO 50001 标准,为压缩空气系统安排一次审计评估。这样一来,企业可以在此基础之上,以非常有针对性的方式,并把钱用在刀刃上,最终满足法律和标准规定的相关要求。同时还能不断提高自身的能源效率。除上述业务以外,近来我们收到的另外一种来自企业询盘也日渐增多——了解机器和设备在大规模改装前后的能效情况。比如安装新压缩机或布设新产线前后。在这两种情况下,审计都能为提高运行效率奠定坚实的基础。审计报告会明确指出哪些方面可以提高设备可靠性——通常是采用一些简单的方法。
Heiko Fleischhacker:压缩空气能效审计在 Mativ Inc 旗下一家公司取得的成效就是个很好的例子。这家公司的压缩机布设尺寸错误,而且缺少上级压缩机控制器。通过改造,我们大幅提高了压缩机的精确度,使其工作时间能够根据实际气压需求进行精准调整。压力调节和能源效率都实现了可持续改善。此外,这些调整还降低了压力波动风险,使系统性能更加稳定。通过系统性消除泄漏,我们还发掘出更多节约潜力。而所有这些措施都有助于实现可持续改善, 不但能降低能源成本,还可延长设备的使用寿命。
Heiko Fleischhacker:是的,当然!维护和维修成本往往与压缩空气系统设计不当有关。在我们执行过的诸多审计中,我发现,只要使用得当,机器的使用寿命绝对能超过 20 年。但是一旦布设错误,机器的使用寿命可能只有 5 年。在审计框架下有针对性地进行优化和定期检查,不但能避免因开发导致高昂支出,还能显著改善设备的整体性能。
Heiko Fleischhacker:审计结果必须得到企业的信任,让客户相信审计结果真实、公正地反映了系统和流程的情况。在这种前提下,保持中立至关重要,因为会直接影响审计结果的可信度和认可度。保持中立是我们这些认证审计员必须履行的义务。这意味着我们要独立、客观地进行审计,不能代表任何个人或企业利益。因此,我们非常重视遵守 DIN ISO 11011 标准针对压缩空气系统能源审计工作规定的具体要求。
Heiko Fleischhacker:我们在气动和电气自动化领域拥有多年专业经验,因此备受客户青睐。早在单个组件开发阶段,我们就非常重视能效问题。但是对我们的客户来说,全方位检查企业的整套系统更有益处—— 在此过程中,不但能发掘节约潜力,还能为更高效地使用压缩空气开发合适的解决方案。Festo 节能服务为感兴趣的企业提供定制服务, 从分析当前现状,到为压缩空气系统和设备现场提供解决方案建议和具体优化措施,不一而足。
在Festo进行压缩空气能源效率审核后,所有结果——从压缩机房的消耗曲线、压缩空气质量到定位的泄漏– ——都集中显示在Energy Saving Services门户网站中供您使用。 这样,潜在的节约和措施就可以永久追踪,并有条不紊地跟进。
申请审计Heiko Fleischhacker:能源效率始于机器和设备的设计与规划阶段。重要的是了解阀的最佳位置,以及软管截短或延长对能耗有无影响。因此我认为,企业从一开始就看重长期节能潜力这一点很重要。比如,装有集成式止回阀的机器购置时可能价格更高一些,但却能在生命周期内,凭借卓越的节能效果快速抵消较高的购置成本。Festo 从项目初期就为客户提供全面的建议。此外,我们还使用先进的模拟工具和数字规划工具,确保系统配置高效且可满足未来需求。借助详细的早期规划,我们在客户开发高性能、高能效系统时为其提供支持。
感谢 Heiko Fleischhacker 围绕生产企业压缩空气能效审计的意义和执行问题提供的广泛信息与宝贵见解。他在专业知识和丰富经验基础上,向我们阐述了企业如何通过压缩空气系统整体审查实现显著节能和能效提升。