Hydrogen is produced via electrolysis – a process in which water is split into hydrogen and oxygen using electricity. An important factor for producing green hydrogen is that the electricity used must come from renewable sources.
This is in contrast to, for example:
That means electrolysis is the first – and crucial – step in the hydrogen value chain.
The starting point in the hydrogen value chain is electrolysis. Water is split into hydrogen and oxygen using electricity from renewable energy sources. Different electrolyser technologies are used depending on the framework conditions:
An automated controller ensures that the temperature, pressure and media flows are always within the optimum range, creating maximum efficiency and plant and system availability.
Freshly produced hydrogen is rarely pure right from the start. It often contains moisture, oxygen residues or other contaminants. Special systems for hydrogen treatment bring it to the required quality – a purity of up to 99.999%. This is crucial in order to prevent corrosion, loss of efficiency or damage to downstream systems. Automated systems monitor all relevant process parameters in real time, react to deviations and optimise the use of energy and equipment. This not only increases safety, but also makes the entire process more efficient and easier to scale.
Hydrogen has a very low energy density at standard pressure. There are several ways to transport or store it efficiently:
Pressure control, filling and monitoring must be seamless and reliable. Precise valve technology and reliable sensors ensure safe, stable operation.
The route from the place of production to the place of use can look very different and includes pipelines, trailers to on-site production. Whatever the method, transport must be safe, low-loss and economical. Automated monitoring systems detect leakages or pressure fluctuations at an early stage and control the flow rate and valve positions in real time.
Green hydrogen has a wide range of applications. It can be used directly as a molecule in the chemical industry and for steel production and is also used in the production of synthetic natural gas or fuels. In fuel cells, hydrogen can then be used again to generate electricity, contributing to low-carbon mobility by reducing CO2 emitted by vehicles. Every application brings its own challenges, but automation technology helps to master them flexibly and reliably. Processes can be adapted to changing conditions and load profiles at any time and meet important safety requirements.
氢能自动化技术复杂,一旦发生故障则代价高昂。 此检查清单可帮助您规避风险,设计出更安全、更具可扩展性的系统。 您将学习到以下内容:
只有安全、可靠、高效地生产和利用绿色氢气,它才能具备市场竞争力。 采用阀岛与模块化控制器的自动化解决方案,结合实时诊断功能,正是实现这一目标的关键。 除其他外,它们还有助于:
Festo 为整个氢能价值链上的企业提供行业特定的自动化解决方案。 无论是在电解、气体处理环节,还是在槽车控制系统等移动应用中,Festo 凭借可扩展的系统、数字化诊断功能及认证组件,助力客户构建安全且面向未来的工艺流程。
它如今已成为现实,且其重要性正与日俱增。 了解整个产业链的,方能做出精准决策,并及早集成合适的解决方案。
想了解更多信息?
您是否正在着手开发某个应用?