For some years, 3D laser scanning has been revolutionizing the ways things are documented and planned in archaeology, architecture and industry. The three-dimensional visualization of buildings and complex shapes enables a more accurate, reliable and faster working method.
Laser scanners, as the name suggests, work with laser light. During a single scanning process, a short sequence of steps is carried out several million times: the scanner emits a laser beam, which is reflected by the surroundings. The scanner’s receiving optics pick the beam back up. The laser light received by the scanner is evaluated using special measuring procedures.
The 3D laser scanner is fastened onto a tripod and rotates slowly around a vertical axis by means of a standard servomotor. A mirror, which rotates around its horizontal axis at several hundred revolutions a minute, deflects the emitted laser beam. In doing so, the laser scans all the surfaces surrounding it in a particular radius, records the intensity of the reflected signal and creates millions of tiny measuring points – up to 976,000 points per second. These measuring points result in an image of the surroundings in the form of a point cloud. The scanner links these points with photos of the real surroundings. The result is an image of the surfaces in three-dimensional space.
借助充当扫描仪方位点的所谓参考球体,可以将多次扫描结果相互连接以创建数字图像,例如建筑物的完整楼层。利用传统的 CAD 程序,可以将对象和设计添加到扫描仪创建的三维图像中。这极大地简化了规划过程。
甚至在新建 Scharnhausen 技术工厂时,Festo 也是借助增材制造工艺(3D 打印)进行规划的。在一个微型工厂里,当施工还在进行时,工人们就能够对他们未来的工作场所有初步的了解。为了实现电子器件制造的现代化,Festo 选择了 3D 激光扫描。这样,就能对未来的工作站进行快速且详细的规划。 规划阶段之后的意外情况、昂贵的调整和延期均得以避免,因为技术建筑系统是根据真实数据规划的,缺失的尺寸能够快速而容易地确定。