ROTAN GmbH was founded in 1987 in Dannstadt near Ludwigshafen, Germany. They now have two additional branch offices in Leuna and Rostock. More than 200 employees develop complete solutions for tank refurbishment, pipe system and plant construction, for instrumentation and control engineering, as well as cleaning technology for customers from many industry segments worldwide.
ROTAN‘s water-based cleaning systems are matched precisely to the requirements of the goods to be cleaned and the necessary degree of cleanliness. ROTAN manufactures GMP/FDA-compliant cleaning systems for the food and pharmaceutical industries. They have to meet demanding requirements for sterility. ROTAN also develops systems for cleaning barrels and containers which come into contact with toxic and highly potent active ingredients. These systems work with a four-step process:
1. Feeding in the stainless steel vessels
2. Opening the vessel lids from a personal safety cabin
3. Cleaning the vessels internally and externally
4. Removing the vessels via a buffer area
Every time the vessels are cleaned, the personal safety cabin and the cleaning chamber must be cleaned and decontaminated too. During normal operation this is done once an hour with water, acid and lye, and under certain circumstances with customer-specific cleaning agents as well.
In these type of cases it is extremely important that the automation components used are sturdy and reliable; every failure or machine stoppage during the cleaning process results in complex, time-consuming intervention. Service personnel therefore have to wear special personal safety equipment because they are at high risk of contamination.
Festo 为该清洁系统的每个过程步骤提供了最坚固的组件,从不锈钢 ISO 气缸 CRHD 到用于空气处理的气源处理单元:
坚固性和耐腐蚀性是清洁系统中所有组件的重要标准,这些组件必须确保在恶劣条件下平稳运行。这适用于所有工业系统,而不仅仅是制药、化妆品和生物技术领域。
借助 Festo,您可以使用种类繁多且非常可靠的优质不锈钢组件。此外,我们还为您选择合适的产品提供支持:使用智能工程工具进行与应用程序匹配的配置,当然还有个人咨询。Festo 的 CAD 数据库也简化了设计工程师的系统规划。ROTAN 快速、简单地创建了良好的系统可用性和操作可靠性。
快速简单意味着供应链精简。在 Festo,您可以从全球范围内的单一来源获得所有组件,包括备件在内的交货期很短。
欢迎询问专家,了解 Festo 可以为您提供的服务。通过此链接分享我们推荐的解决方案和示例应用程序。
Riedstr. 3
D-67125 Dannstadt
Germany
业务领域:为管道系统和工厂建设、储罐清洁、仪表和控制工程以及清洁技术开发完整的解决方案