Casting resins protect high-quality electronic components against undesirable penetration by dirt and moisture. Precise and reliable dispensing technology is essential for the automatic application of these resins. bdtronic GmbH, a company located in Weikersheim in Baden-Württemberg, is one of the world’s leading suppliers of dispensing systems, including complete systems for automating the assembly and production of electronic components. bdtronic has now worked with Festo on a groundbreaking project to expand its product portfolio. The new mini-dis from bdtronic, based on the compact handling system YXMx, opens up another field of application in the front-end processing of electronic and telecommunications products. The integrated CECC-X controller allows curved travel paths, thus making it possible to produce even complex casting patterns. Designed as a space-saving and flexible desktop application, the new complete solution from Festo facilitates cost-effective production of extremely short production runs.


Precision and reliability
The microdispensers and the mini-dis are used with semiconductor products and circuit boards, with the electronic components of numerous automotive modules and sensors, in medical technology and with smartphones. The mini-dis processes single- or two-component materials with an epoxy, polyamide, silicon or acrylate base as well as soldering pastes in the µl range. Across the world, several thousand different casting materials are used.
When it comes to the dispensing technology itself, two criteria are especially important: precision and process reliability. To achieve these, bdtronic works extremely closely with its clients’ experts. In the company’s own application and technical centre, each product is extensively tested to check the interaction between the casting resin, the dispensing technology and the components to be processed. One of the greatest challenges in the dispensing process is the optimum preparation of the casting resins. These must first be homogenised and then evacuated. This avoids even the smallest air pockets.

Flexible and compact

An important criterion for bdtronic when selecting handling systems for dispensing is an interpolated actuator control system which allows travel along radii and thus flexible contours. This is the only way to define precise dispensing points, create intricate patterns and fully encapsulate components of different shapes. The new desktop application with a Festo controller CECC-X with SoftMotion functionality fulfilled this need. A key role was played by the programming language CODESYS, with which the bdtronic software engineers had already been working for many years. Since the CECC-X can be integrated via CODESYS, it could be added to the company’s component family in no time at all. A further important criterion is easy reading-in and fast processing of CAD data.

With its compact dimensions, the controller is a perfect match for the planar surface gantry EXCM-30, which offers many functionalities for payloads of up to 3 kg. The gantry provides maximum working space coverage. And it can travel to any required position within the working space.

Perfectly matched

Festo has designed its compact handling systems as a kit with perfectly-matched standard components. The bdtronic mini-dis uses a planar surface gantry EXCM-30 with additional Z-axis EGSK as a kinematic mechanism including the controller CECC-X. It also includes a comprehensive software package for simple programming and commissioning, which is an integral part of the Festo complete solution. Having a large number of functions available in a very small space avoids the problems of both under- and over-dimensioning. The controller software, based on CODESYS, offers the most important basic functions that are needed to program travel paths even without an in-depth knowledge of programming. The controller interfaces allow the compact USB cameras, sensors, actuators and valves all to be connected. All of this results in great efficiency and saves considerable amounts of time and money.

运动装置、控制器和软件集成到一处

用于移动工件或工具的紧凑型抓取系统有助于电子产品和小型零件制造领域的机器和系统制造商大幅降低其工程成本,此外由于采用了标准组件,还可以实现成本效益。软件库中的预定义功能模块和带有定序器的直观应用程序编程可简化编程和调试流程。

系统中完美匹配的元件和功能都来自 Festo 单一货源。这些组件可用于简单地组合完整系统,包括运动装置、控制器甚至软件。此类系统为节省开支开辟了全新的可能, 使机器和系统制造商能够完全专注于其核心业务。

使用 Handling Motion Lib 的预定义功能模块可以轻松快速地进行编程和调试, 并可实现以下功能:用于与主机系统进行通信的接口参数化、参考行程和反复起动操作,用于故障处理和顺序处理的文件管理和消息系统。

系统套件中包含一个紧凑型控制器 CECC-X, 用于在有限的空间中执行多种功能。其中包含主控制系统的一系列预定义接口,也包括用于 Industry 4.0 的 OPC-UA 接口。

bdtronic GmbH

Ahornweg 4
97990 Weikersheim
Germany

www.bdtronic.de

业务领域:在点胶技术、等离子预处理、热封、浸渍技术和过程自动化领域提供完整解决方案。