Since 2016, premium manufacturer Scania has been assembling customized truck cabs to order – and doing so almost exclusively with the aid of 288 robots. "It's completely clear to me that a premium product needs to be built in a premium plant," explains Marcus Holm, Plant Manager in Cab Body Production at Scania in Oskarshamn. "The high degree of automation results in excellent quality, as well as good working conditions and ergonomics for our operators," he adds.
The robots place the panel parts on the joining stations and weld them. All the employees have to do is load the stations and monitor the machines. In any case, Swedish occupational health and safety regulations have made it impossible to use hand-held welding equipment. On the one hand, welding tools have become too heavy and unwieldy, while on the other hand occupational safety directives require a minimum distance between the welding gun and the operator because of radiation.
The banning of manual welding from the assembly workshop has benefited Scania in two ways: "It means better processes and quality," explains Lars Kreutner, Project Leader Cab Body Production at Scania in Oskarshamn. To make full use of the automation technology, Scania has set up a training division where employees learn how to use the robots and automation technology.
All the trucks that Scania builds weigh more than 16 tons. The company has built a reputation as a manufacturer of special vehicles for fire services or waste collection, for example. These niche markets alone account for hundreds of thousands of variants.
"It may surprise people to learn that we offer even more customization options for trucks than there are in passenger car production," says Evert Forsberg, Automation and Electrical Engineer in the press shop and body shop at Scania. In passenger car production, every vehicle type has its own assembly line. "We, on the other hand, assemble all of the cabs that Scania supplies on a single assembly line," says Forsberg.
这意味着该车间拥有工业物联网的许多关键特性 — 定制车辆的大规模生产、控制技术带来的适应性和灵活性、诊断能力以及工业能效和安全解决方案。“所有工厂制造商都有一个模块化标准化概念,”Forsberg 说。归根结底,工厂操作员需要能够依赖成熟的自动化产品。另一个目标是避免不必要的备件库存。所有面板都在气动驱动装置中夹紧,然后进行焊接。"自动化专家 Forsberg 说:“我们决定选择 Festo 的预配置型 CPX/VTSA 阀岛,是因为它们具有许多好处 — 例如以太网接口和网络接口、诊断、安全、PROFINET 和工业能效。"
CPX/VTSA 阀岛实际上是 PROFINET 的唯一接口 — 不需要额外的接线。阀岛通过自动化平台 CPX 提供诊断数据,并可用于监控系统,作为预测性维护的一部分:“我们可以在系统组件出现故障并使整个系统瘫痪之前更换它们,”项目经理 Kreutner 解释道。
“我们也对阀岛的安全概念印象深刻,”Forsberg 说。当需要干预时,CPX 可以在不同的压力区和排气区进行操作。"我们可以使用移动面板检查受影响的系统部件,而不必搜索整个系统来查找错误 — 那就像大海捞针一样。" 此外,对单个系统部件重新加压比启动整个系统更节能。
焊接机器人需要压缩空气来移动焊枪和夹紧金属板材。冷却水防止焊接系统过热。Festo 为焊枪提供完整的压缩空气和冷却水供应解决方案。在 Scania,它们集成在安全围栏中,便于操作 — 包括 MS 系列气源处理。
对于静态焊枪,Festo 开发了完全符合 Scania 和 ABB 规范的旋转臂,在完成 150 个点焊后,旋转臂将电极铣削装置,即所谓的电极研磨器,带到电极上。旋转臂由 Festo DNCE 电缸精确定位,并由 EMMS 步进电机驱动。利用该解决方案,Festo 将周期时间缩短了一半以上。
其原因是焊枪电极在使用时变钝,必须在大约 150 次点焊后铣削,以确保点焊完全准确。“电极铣削的原理和钝铅笔的削尖一样,”Festo 负责 Scania 的前大客户经理 Leif Lindahl 解释道。
Festo 用于电极铣削的控制柜包括 CMMS 电机控制器和 CPX,后者与电机控制器和主机器人控制器通信。“安全性也有所提高,因为工厂操作员在铣削后不再需要进入机器人单元来调整电极到点焊的正确位置,”Lindahl 补充道。
Scania is ushering in a new era in vehicle manufacturing in Oskarshamn. As it is almost completely automated, but still allows huge flexibility right down to a batch size of 1 on a single assembly line, the body shop is already well on its way towards the Industrial Internet of Things. The new factory has set a precedent, and Scania will shortly build a similar factory at the Scania plant in São Paulo, Brazil.
Oskarshamn is an industrial town on Sweden's east coast, around 300 km south of Stockholm, with transport links to the holiday islands of Gotland and Öland. In 2017, a workforce of 2700 assembled a wide range of cabs for all Scania models here. Vehicle transporters take the cabs from Oskarshamn and deliver them to the Scania assembly plants in Södertälje near Stockholm, Zwolle in the Netherlands, and Angers in France, where they are assembled to create the complete truck chassis.
A Volkswagen Group company
151 87 Södertälje
Sweden
Key activities: Heavy commercial vehicles (trucks and buses), marine and industrial engines