午夜时分, 烟花照亮夜空, 软木塞弹出瓶口,在空中飞舞——有时运动速度会超过每小时 45 公里,比短跑名将尤塞恩·保特跑得还快。这是新年前夜的经典场景。根据调查,大约 78% 的德国人,甚至 94% 的奥地利人都同意,举起一杯起泡酒已经成为了庆祝新年的标志。其中有一半的人更喜欢名字鼓舞人心的起泡酒, 例如凯斯勒起泡酒。借助新的酿造系统和经过优化的流程,这家德国最古老的起泡酒生产商希望进一步提高质量标准,从而为未来的增长奠定健康的基础。而 Festo 培训和咨询公司的专家可以帮助他们实现可持续发展。
传统起泡酒酿造商凯斯勒的执行合伙人 Christopher Baur 说道:“我们最近在先进生产设备上进行了巨额投资,以在未来几年内大幅度提高产量,达到 150 万瓶左右。” 1826 年,为世界上最著名的法国香槟酒酿造商之一工作多年之后,Georg Christian von Kessler 在埃斯林根创立了同名的起泡酒窖。回到德国后,他带来了一种非常特殊的香槟酿造工艺:“传统法”(méthodeTraditionalelle),这是一种瓶内发酵工艺,至今仍用于酿造该公司的顶级起泡酒。
在时间的作用下静置发酵
在过去的 190 年中,凯斯勒以其不折不扣的产品质量闻名于世。“到目前为止,我们 90% 的酿造工艺都依靠瓶内发酵。所有酒瓶仍然存放在我们建于 13 世纪的历史建筑中,在某些情况下,还存放在中世纪的老窖中。”Christopher Baur 自豪地解释道。先在木桶中进行发酵,然后在瓶中进行二次发酵:静置的酒就变成了起泡酒——根据酒的种类,陈酿时间可能长达五年。优质起泡酒的秘密在于时间——这种说法是有道理可言的。说到时间,由于起泡酒的消费需求不断增加,酒窖的规模也在稳定扩大。为了能够大规模使用传统的复杂生产工艺,凯斯勒最近购置了现代化的机器,如今这些机器已用于生产子过程中。例如,在除去酵母时,要从瓶子中除去酒糟(其中包括酵母和沉淀物),然后进行包装。包装过程包括塞入软木塞和贴上标签,然后精美的瓶装起泡酒就可以上市了。
Premium processes for premium products
But the use of new systems also means different work processes and changing requirements for employees. “To be able to ensure top-quality and consistent growth, the organisation behind the scenes has to be adapted too. And so it was important for us to have external professionals to carefully examine, analyse and optimise our processes,” explains Baur. Kessler counts on the long-standing expertise of Festo Training and Consulting with the goal of improving efficiency in production. “We want to produce our premium products with premium processes,” says Baur, getting to the heart of the matter. It all started with a strategy workshop facilitated by Festo, for managers, supervisors, and selected employees from production, sales, and logistics at Kessler. Among other things, a business game was used to develop a feeling for the entire value creation chain. This was followed by an in-depth value stream analysis. At the end, a comprehensive concept evolved for the long-term optimisation of all production steps – including employee training sessions. In keeping with the motto: an even more sparkling or rosé(y) future with more fluid processes.
“Implementation is going very well, as is collaboration with the team from Festo headed up by Project Manager Ulrich Fischer. We don’t see it as a purely strategic project, but rather as an operational project. That is why it’s been very important for us to closely involve our employees and provide them with optimal training,” says Baur, whose company is dedicated to continuous development despite its long history: “Learning needn’t be a contradiction to tradition – and tradition must evolve as well.” And the best source of inspiration for evolution is plentiful at Kessler, as US author Mark Twain once said: “Champagne is indeed the most joyous source of inspiration.”
KESSLER Sekt GmbH & Co. KG
Georg-Christian-von-Kessler-Platz 12-16
D-73728 Esslingen am Neckar
www.kessler-sekt.de
Area of business: Production of sparkling wines