The store will not work correctly in the case when cookies are disabled.
Festo uses cookies to improve performance, optimise functionality, analyse access and personalise content and displays. You can disable the use of cookies at any time. For more information, please see our Data Protection Policy and Cookie Policy.
These include cookies that enable Festo to optimise the website based on users' behaviour (tracking) and are stored anonymously.
These cookies assist users in that optimum suggestions are made based on users' behaviour.
These cookies enhance the functions and convenience of the website. For example, encrypted user data can be stored in them for an automatic logon. These cookies can be stored for a long time.
These cookies are used for enabling the basic function of the Festo website and the online shop. These cookies cannot be deselected.
The starter package covers various motion apps for different applications. The starter package light contains the most important pneumatic basic functions and is intended for Festo Motion Terminals without input modules.
Description
The starter package covers various motion apps for different applications. It contains the most important pneumatic basic functions.
Motion apps within the starter package can be used in parallel and without restrictions on each valve of a Festo Motion Terminal VTEM.
The following motion apps are part of the starter package: