Why is bin picking so important in intralogistics?

Arquemino Lopes Junior: The increasing variety of products, the ongoing boom in e-commerce and the growing complexity of logistics processes require intelligent automation strategies. Companies need to work more efficiently and cost-effectively in order to remain competitive in this environment. Bin picking is the automated part of intralogistics. It enables companies to remove a wide variety of objects precisely and reliably from chaotic or organised containers. With this technology the flow of materials can be optimised and bottlenecks in the logistics chain can be avoided.

What challenges, opportunities and risks do you see in this context?

Arquemino Lopes Junior: The big challenge is to develop gripper systems that can flexibly and reliably grip a variety of different items. A system that can really grip any object is like searching for the Holy Grail. The variety of product geometries and materials poses an enormous challenge for automated gripping. If the bin-picking process is not frictionless, it quickly becomes a bottleneck in intralogistics. The risk is that the material flow comes to a standstill and the performance of the overall system is reduced. On the positive side, companies that successfully integrate intelligent bin picking into their processes are taking a decisive step in the right direction. They not only boost their efficiency, but also create the basis for surviving in a market that demands ever faster and more flexible solutions.

您认为市场中的哪些因素是这项技术的主要发展推手?

Arquemino Lopes Junior:在线购物无疑是当前智能仓储挑战的最大驱动力。疫情有力推动了电子商务的发展,虽然疫情后增长有所放缓,但仍然保持着积极和持续的态势。不断增加的订单量也大大提升了物流处理需求。这一发展伴随着产品日益多样化,导致散乱零件抓取过程中需要处理更多不同的产品几何形状和材料。

消费者期望也起到了决定性作用。他们希望所订购的产品能够迅速到达我们手中,最好是当天送达。这种期望使企业面临额外的挑战,需要更快地处理本已庞大的电子商务订单。正是在这方面可以清楚看到,智能和自动化散乱零件抓取不可或缺,它能够确保效率、速度和可靠性。

近年来哪些技术发展对散乱零件抓取技术产生了重大影响?

Arquemino Lopes Junior:在我们看来,主要有三项技术发展改变了散乱零件抓取:人工智能和机器学习的影响、图像处理和物体识别的进展,以及实时数据的使用。这些技术显著提高了系统的精确性和灵活性。

最重要的目标仍然是计算出最为合适的抓取点,并将“手臂端”的抓取系统设计得尽可能高效。为了将抓取错误降到最低程度,Festo 将气动、电气和数字自动化的所有优势应用到寻找解决方案中。

我们抓手技术产品系列种类丰富,能够涵盖大量应用场合。特别要强调的是我们的定制解决方案。这些方案通过与客户进行有针对性地合作而开发得来,用以开放适应个性化需求的抓手解决方案。在我们发起的“Grip it”开发倡议框架下,一个跨国团队通力合作,专门致力于开发特殊抓手。

GripperAI – Intelligent Gripping with Artificial Intelligence​

GripperAI is an innovative software solution from Festo that has been specially developed for bin picking. It enables bin-picking robots and handling systems to pick up disorganized objects of different shapes precisely and flexibly. Thanks to artificial intelligence, the solution learns autonomously, adapts flexibly to new tasks, and thus optimizes the efficiency of your intralogistics. GripperAI can be easily integrated into existing automation environments. Get an overview of the most relevant aspects and interesting insights in our White Paper.​

Download white paper

如何利用自动化过程中的数据来优化智能仓储效率?

Arquemino Lopes Junior:一个很好的例子是预测性维护 (Predictive Maintenance)。许多客户使用我们的创新软件 Festo AX 处理其机器设备中的实时数据,并通过人工智能进行分析。这样将停机时间减少高达 25%,并持续提升生产效率。在电气自动化领域,我们也同样依赖 Festo AX。通过分析电机的电力消耗,我们能够了解电机一天中的工作情况。能耗峰值通常表明转矩需求增加以及存在机械问题。通过 Festo Ax,我们能及早发现性能下降的原因,防止潜在故障,避免产生问题。实时数据还使我们能够清楚了解,所有组件是否合适,其尺寸设计是否正确。这样能够提高效率、将磨损减小到最低程度、延长设备使用寿命,并降低运营成本。

Festo 如何通过 GripperAI 支持现代智能仓储的要求?

Arquemino Lopes Junior:GripperAI 绝对是一项针对散乱零件抓取的创新。通过这项革命性软件解决方案,我们能够使机器人和搬运系统精确灵活地抓取不同形状和尺寸的无序物体,即使它们的摆放处于混乱状态。我们的解决方案利用人工智能,尤其是机器学习,来自动适应不断变化的抓取任务,持续优化抓取过程中的效率。因此我们不再需要 CAD 模板来配置摄像头或进行耗时的机器人示教。GripperAI 能够自主识别物体,并根据实际情况计算最佳抓取点。这增加了解决方案的灵活性,并大大减少了手工操作量。

测试中,GripperAI 在简单任务中几乎达到了 100% 的成功率。即使在物体无序、环境混乱的复杂场景中,成功率都同样很高。这表明软件能动态地适应不同的要求。

基于人工智能的箱内抓取,实现灵活的流程

通过创新的人工智能为您的智能仓储效率制定新的标准。Festo 的解决方案可以帮助您全自动抓取不同形状和尺寸的无序物体。GripperAI 是 Festo 专为智能仓储中的散乱零件抓取而开发的创新软件解决方案。

了解更多

GripperAI 已应用在哪些方面,计划有哪些进一步发展?

Arquemino Lopes Junior:目前,我们在多个试点和研究项目中使用 GripperAI 来测试新功能和应用。我们与物流企业合作,使用该技术试验抓取不同部件 - 从小物件如 USB 闪存盘或罐头到大物件如重型纸箱。

我们未来的扩展计划旨在进一步提升该软件的学习能力和适应能力。这还包括集成附加的传感技术和图像处理技术,以进一步优化抓取过程的精确度和效率。研究项目 FLAIROP 需要重点介绍。在这个项目中,我们研究如何通过使用集成摄像头和分布式人工智使抓手变得更加灵活和智能。我们的目标是跨地点利用训练数据,同时不泄露敏感的企业数据。

您会给那些想要将散乱零件抓取集成到生产流程中的企业什么建议?

Arquemino Lopes Junior:务必选择一个具有广泛自动化专业知识并拥有丰富抓手技术产品组合的合作伙伴。只有这样,才能开发出满足特殊应用需求的解决方案。而标准解决方案在散乱零件抓取领域往往有其局限性。在许多应用领域有着各种不同的个性化要求和条件,定制解决方案是必须品。因此,您的合作伙伴应该愿意与您共同开发个性化解决方案。

由于许多机器常常在不同的国家使用,选择一个全球范围内布局的自动化合作伙伴至关重要。这不仅保证备件的供应,还能确保系统的顺畅运行。

也许最重要的建议是选择一个跨技术开发并提供一揽子解决方案的合作伙伴,他能够提供气动、电气以及数字化解决方案。采用哪种技术始终取决于相应应用的要求。一个在各个领域都具有专业能力的合作伙伴,能够帮助您根据自身工业流程打造自动化战略。

感谢 Arquemino Lopes Junior 围绕散乱零件抓取在智能仓储中的重要性,为我们提供了丰富的信息与宝贵的见解。他在专业知识和丰富经验基础上,向我们阐述了企业如何通过自动化“散乱零件抓取”实现显著能效提升。