• Products
  • Downloads

Circuit diagram service from Festo: a finished EPLAN project in just a few minutes

There are countless files accumulating on computers. With Schematic Solution, Festo has developed a service that creates a project using the order code for a custom configured solution. And in no time at all!

Simply enter the order code in the search field and you will receive the complete plan in just a few minutes – error-free and trouble-free. No more tedious searching for, downloading and piecing together individual components.

How to work with Schematic Solutions

Festo has been supporting work with EPLAN for many years. EPLAN documentation with Schematic Solutions is therefore simple and error-free. If you use ‘EPLAN Electric P8’ or ‘EPLAN Fluid’, Festo can provide you with macros in 21 languages for more than 38,000 components. Top service. Top results.

Save time!

Why use up the time of a well-paid engineer to do less than productive tasks when there is a service to do this work? Documenting an EPLAN project manually can take several hours and, depending on the complexity, is very error-prone. Schematic Solution allows you to use this time to add value and create project documentation without any errors.

Step 1: Log in and configure

  • Log in to the Festo App World
  • Load the Schematic Solutions app
  • Enter ID codes from the order

Step 3: Store

  • Load the Schematic Solutions app
  • Enter ID codes from the order

Step 2: Log in to the Festo App World

  • Log in to the Festo App World
  • Load the Schematic Solutions app
  • Enter ID codes from the order